Technical FAQs

Ask a Question

What is the difference between an Illuminated beacon and an illuminated indicating bank ?

Beacons are single illuminated units that have a domed lens on top, they are not stackable. Indicating Banks have stackable components ( steady , flashing or strobe lights and sounders ) . Some strobes have domed lenses and these can only be located in the topmost position in the Bank . Bulbs and some accessories are interchangeable between Beacons and Banks of the same family .

CTA-ID : 2049713
Was this helpful?
What can we do to improve the information ?