Technical FAQs

Ask a Question

What is the voltage tolerance of the coil in the CAD relays?

For AC 85 to 110% of the nominal coil voltage at 60hz , 80 to 110% of the nominal coil voltage at 50hz. For DC 70 to 125% of the nominal voltage for standard and low consumption units.


CTA-ID : 2049705
Was this helpful?
What can we do to improve the information ?