Technical FAQs

Ask a Question

On an LEL type circuit breaker lug which permits multiple conductors per lug, can two different sizes of wire be landed? For example, a 4/0 and a 2/0 wire?

No. Standard lugs must always use the same size wire if more than one of them are used.


CTA-ID : 2049567
Was this helpful?
What can we do to improve the information ?