Technical FAQs

Ask a Question

Catalog number LDGB8A is obsolete. Is there something that will replace this wireway adapter?

Yes. Catalog number LDB8A is available, which is made of regular steel rather than galvanized steel.


CTA-ID : 2049507
Was this helpful?
What can we do to improve the information ?