Technical FAQs

Ask a Question

Customer has a LC1F400 and is having a problem direct mounting the LR9F7379 overload.

Completely remove the screws, two per pole, that secure the busbars passing thru the outer legs of the overload. Remove and rotate the outer busbars 180 degrees and re-install securing them with the screws.


CTA-ID : 2049462
Was this helpful?
What can we do to improve the information ?