Technical FAQs

Ask a Question

Can the QOB Bolt-On type branch circuit breakers be used in QO load centers?

Issue:
Product design

Product Line:
QO Load centers

Environment:
Branch breakers

Cause:
Application

Resolution:
QOB Bolt-On circuit breakers cannot be used. QO load centers will ONLY accept QO Plug-On type branch circuit breakers.


CTA-ID : 2049717
Was this helpful?
What can we do to improve the information ?