Technical FAQs

Ask a Question

What are the repair parts for a QO420L125, Series G1, Three-phase Load Center.

Issue:
Old design repair parts

Product line;
QO load centers 

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC420LF/S - OBSOLETE
Interior Assembly - QON420L125 - OBSOLETE
Neutral Bonding hardware - 4028330450 - OBSOLETE
Main Lugs - 4025109450 - OBSOLETE
Neutral Assembly - SN20
Indoor Cover mounting screw - 4020513002K
The following repair parts are obsolete and no longer available:
Indoor cover door hinge - 173132
Indoor cover latch ring - 186012
Indoor cover latch spring - 163471


CTA-ID : 2049645
Was this helpful?
What can we do to improve the information ?