Technical FAQs

Ask a Question

Can the 9039XG1alternator be wired so that both motors will not run at the same time?

This can be done simply by not using a second 2 pole pilot device ``B``. If only the ``A`` pilot device is used, the unit will only alternate the motors.

CTA-ID : 2049437
Was this helpful?
What can we do to improve the information ?