Technical FAQs

Ask a Question

What is the operating temperature of the XCS type safety interlocks?

The XCS safety interlock line is ( -25 degrees C to 70 degrees C), XCSE is ( - 25 degrees C to 40 degrees c), XCSTE is (-25 degrees C - 60 egrees C)


CTA-ID : 2049421
Was this helpful?
What can we do to improve the information ?