Technical FAQs

Ask a Question

What is the warranty for QO and HOM Circuit Breakers, Load Centers, and CSED devices, in a residential application?

Issue:
What is the warranty period for QO and HOM (Homeline) Load Centers, Circuit Breakers, and CSED devices, specifically in a residential application?

Product Line:
QO and HOM Load Centers, Circuit Breakers, and CSED devices

Environment:
Applies to:
  • Residential applications only
  • QO and HOM Load Centers and CSED, single-phase devices
  • QO, QOT, HOM, and HOMT Circuit Breakers used in the above (includes breakers with suffixes GFI, AFI, CAFI, PCAFI, DF, PDF)
  • Does not apply to three-phase devices, or QOB or QOU circuit breakers
Resolution:
I. Square D/Schneider Electric QO Brand Load Center and Load Center Branch Circuit Breakers
Square D QO brand load centers and Square D breakers. Square D warrants its branch circuit breakers to be free from defects in
material and workmanship under normal care and proper usage in a residential installation, for the lifetime of the load center in which
it is installed. QO brand load centers are also covered under the same lifetime warranty. If the circuit breaker or QO brand load center
fails within the warranty period because of a defect in material or workmanship, Square D/Schneider Electric will replace the defective
breaker or device free of charge upon following the notice procedures below and return of the product to place of purchase. Exclusive
Remedy — The repair and/or replacement of defective products is your sole and exclusive remedy.

II. Square D/Schneider Electric Single-Phase Load Centers and Combination Service Entrance Device (CSED)
Square D Homeline brand single phase load centers and combination service entrance devices. Square D warrants its Homeline
single phase load centers and combination service entrance devices to be free from defects in material and workmanship, under
normal care and proper usage in a residential installation, for a period of ten (10) years from the date of installation. If the product fails
within the warranty period because of a defect in material or workmanship, Square D will, at its option, repair or replace the defective
part or parts upon following the notice procedures below and return of product to place of purchase.

To see a copy of this warranty in our Retail Catalog, click this link: Retail Catalog 2013
Was this helpful?
What can we do to improve the information ?