Technical FAQs

Ask a Question

What Catalog Numbers for the 200 amp combination service entrance devices have Field Installable CT provisions for use with Photovoltaic system applications?

Issue:
Current product design

Product Line:
Combination Service Entrance Devices

Environment:
CT provisions for use with PV applications

Cause:
Application

Resolution:
There are many of the current design Square D CSEDs that have CT provisions for Photovoltaic system applications. SEE THE CURRENT ON-LINE DIGEST PAGES
1) Page 1-25, table 1.59 for the SC2636M200_225FPV
2) Page 1-30, table 1.66 all the devices in this current table have provisions for Field Installed CTs.
3) Page 1-31, table 1.68, all the devices in this current table have provisions for Field Installed CTs.

NOTE: PLEASE Note that digest page numbers and tables can and will change, SO ALWAYS make sure to check the information for EACH catalog number in the digest BEFORE obtaining the devices.




 
Was this helpful?
What can we do to improve the information ?