Technical FAQs

Ask a Question

What is the part number for a 200% neutral assembly for a J250DS circuit breaker enclosure?

For a 200% neutral application, use SN400LA, dependent upon the quantity and size of neutral conductors being used. The SN400LA will accept (1) #1 AWG - 600 KCMIL or (2) #1 AWG - 250 KCMIL AL/CU conductors IN and OUT.

CTA-ID : 2049664
Was this helpful?
What can we do to improve the information ?