Technical FAQs

Ask a Question

What is the part number for a 200% neutral assembly for an LX600AWK circuit breaker enclosure?

For a 200% neutral application, the SN1000MA solid neutral assembly may be applicable, dependent upon the quantity and size of neutral conductors being used. The SN1000MA accepts (3) #3/0 AWG - 500 kcmil aluminum or copper conductors IN and OUT.

CTA-ID : 2049657
Was this helpful?
What can we do to improve the information ?