Technical FAQs

Ask a Question

What is the current draw for the AC and DC undervoltage trips for the Powerpact H and Powerpact J breakers?<br />

All Powerpact H and J - AC voltage undervoltage trips have a pickup consumption of less than 10VA. All Powerpact H and J - DC voltage undervoltage trips have a pickup consumption of less that 5 watts.
The continuous hold-in power consumption for AC and DC units is 5 Watts.



CTA-ID : 2049649
Was this helpful?
What can we do to improve the information ?