Technical FAQs

Ask a Question

What is the difference between voltage codes F6 and F7?

On Telemecanique devices with a voltage code the last digit defines the frequency with -5 = 50hz, -6 = 60hz and -7 = 50/60hz. In the question, F6 = 110v 60Hz, F7 = 110v 50/60Hz

CTA-ID : 2049556
Was this helpful?
What can we do to improve the information ?