Technical FAQs

Ask a Question

What is the difference between a HRK30 and HRK30H Class R Fuse Kit?

The HRK30 Class R Kit is used with 30A (Series E) safety switches rated 240V and the HRK30H Class R Kit is used with 30A (Series E) safety switches rated 600V.


CTA-ID : 2049337
Was this helpful?
What can we do to improve the information ?