Technical FAQs

Ask a Question

Can a hub be added to a QO2000NRB?

Yes, It will accept a B type hub 2.5`` maximum. Refer to page 1-17 in the Digest 174 for hub selection.


CTA-ID : 2049335
Was this helpful?
What can we do to improve the information ?