Technical FAQs

Ask a Question

The customer has 8539SBW11, what is the part number for the reset button?<br /><br /><br />

The complete, door mounted, external reset mechanism assembly requires the following parts:

Qty 1 - 30019-114-90 Reset sub-assembly (does not include the ring nut or boot listed below).
Qty 1 - 30019-121-01 Ring nut.
Qty 1 - 9066 W1 Protective boot (also serves as gasket) (required on
NEMA 4X enclosures).




CTA-ID : 2049505
Was this helpful?
What can we do to improve the information ?