Technical FAQs

Ask a Question

What are the voltage limits for a 24volt coil for a RPM relay?

For the 24vdc or 24vac the minimum limit is 19.2 volts and the maximum is 26.4 volts.


CTA-ID : 2048493
Was this helpful?
What can we do to improve the information ?