Technical FAQs

Ask a Question

Can the 400A Meter Mains or All-In-One be retrofitted to include a bypass by using a stud, lever, horn, or manual link type bypass kit?

No. The 400A Meter Mains and All-In-Ones are UL listed as configured when they leave the factory. There is no bypass retrofit kit available.

CTA-ID : 2048463
Was this helpful?
What can we do to improve the information ?