Technical FAQs

Ask a Question

Are Powerpact H frame circuit breakers switch duty rated?

Issue:
Do Powerpact H frame circuit breakers have SWD (switch duty) ratings? 

Product Line:
Powerpact H

Environment:
Electrical distribution

Cause:
Powerpact used for switching flourescent lighting

Resolution:
Some of them are.  SWD switch duty rating on these breakers applies only to 15 and 20 A / 277 Vac or less, 2P and 3P breakers.

 
Was this helpful?
What can we do to improve the information ?