Technical FAQs

Ask a Question

What are the part numbers for the operator or contacts on the XD4PA/XD5PA joysticks?

Issue:
What are the part numbers for the operator or contacts on the XD4PA/XD5PA joystick?

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 Push Buttons

Cause:
Part number is trying to be identified for application.                                                      

Resolution:
Check the system before ordering. Not all of these listed parts are loaded on the system.
The handle assemblies are as follows.
For the XD4 units:
ZD4PA12 2 direction, stay put
ZD4PA22 2 direction, spring return to zero position
ZD4PA14 4 direction, stay put
ZD4PA24 4 direction, spring return to zero position.
For the XD5 units:
ZD5PA12 2 direction, stay put
ZD5PA22 2 direction, spring return to zero position
ZD5PA14 4 direction, stay put
ZD5PA24 4 direction, spring return to zero position.
The contact block/body assemblies are as follows.
For the XD4 units:
ZD4PA103 for 2 direction controllers
ZD4PA203 for 4 direction controllers.
For the XD5 units:
ZD5PA103 for 2 direction controllers
ZD5PA203 for 4 direction controllers.
Was this helpful?
What can we do to improve the information ?