Technical FAQs

Ask a Question

What is the replacement main circuit breaker for a QOBW20M100-1 load center?

Repair parts

Product Line:
Obsolete QO LC


The QOBW20M100-1 is the box reference number, not the load center catalog number. This box was used with the QO12M, QO16M and QO20M load centers. These load centers used the Q12100TF, main circuit breaker, which is Obsolete with no replacement.

CTA-ID : 2048338
Was this helpful?
What can we do to improve the information ?