Technical FAQs

Ask a Question

Is a a breaker with a Micrologic trip unit available in a circuit breaker branch feeder bucket for a Model 6 MCC?

Issue:
Is a a breaker with a Micrologic trip unit available in a circuit breaker branch feeder bucket for a Model 6 MCC?

Product Line:
PTEQP - LV EQPT (IEC & NEMA).

Environment:
Products sold in the United States.

Cause:
Availability.

Resolution:
Yes. Branch feeder buckets are available with Micrologic breakers installed. They must be ordered as a special using the Product Selectors program in Electronic Quote Management.


CTA-ID : 2048426
Was this helpful?
What can we do to improve the information ?