Technical FAQs

Ask a Question

What is the length of a VZ31 shaft extension?

This shaft is suitable for a mounting depth of 5.5`` minimum to 17`` maximum as measured from the front side of the panel to the outside of the door.


CTA-ID : 2048367
Was this helpful?
What can we do to improve the information ?