Technical FAQs

Ask a Question

What is the replacement main breaker for a QOBW20M100-4 load center?

Repair parts

Product Line:
Obsolete QO LC


The QOBW20M100-4 is the box reference number, not the load center catalog number. This box was used with the QO12-20MW, QO14-20MW and QO16-20MW load centers. These load centers used the Q12100TF main circuit breaker, but it is Obsolete, with no replacement.

CTA-ID : 2048340
Was this helpful?
What can we do to improve the information ?