Technical FAQs

Ask a Question

Do we have any 2 inch pipe connections for a 9038CG31?

No alternate pipe connections are available on 9038CG switches. Standard is a bushing 1/2`` to 2 1/2``. However, the bushing can be replaced
by an alternative, although bushings smaller than 2 1/2`` will not allow the float to pass through the threaded opening. In that case, the float must
be attached to the end of the rod after the rod and sealing tube are threaded into the side of the tank.


CTA-ID : 2048577
Was this helpful?
What can we do to improve the information ?