Technical FAQs

Ask a Question

Is there a differennt circuit breaker bus plug catalog number required for a 208/120v application versus a 480/277v application?

No. The circuit breaker bus plugs are rated for 600 volt max applications. The system voltage will determine if a 3-wire or 4-wire plug is needed but it does not directly impact the part number.

CTA-ID : 2048295
Was this helpful?
What can we do to improve the information ?