Technical FAQs

Ask a Question

Do the 600amp Double Throw Safety Switches come standard with a Dual Cover Interlock Feature?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Cover interlocks

Cause:
Application

Resolution:

Yes, the switches are supplied with a dual cover interlock. With the switch in either of the ON positions, the cover cannot be opened. There is no defeat mechanism for this feature. With the switch cover open and the switch in the OFF position, the switch cannot be operated to either of the ON positions. There is a defeat mechanism to allow this feature to be over ridden.


CTA-ID : 2048567
Was this helpful?
What can we do to improve the information ?