Technical FAQs

Ask a Question

What are the repair parts for an EZM382R, Series 004, Branch Unit?

Only the parts listed below are considered field replaceable:

Parts include Meter Socket through Tenant Circuit Breaker Compartment, include quantities for one position only (where a part number only is given the order quantity for that part is one):

Substitute 5-Jaw Meter Socket (supplied with a 4-jaw socket) - 4052720650
Meter Socket Jaw Assembly - (4) 4052706950
Keps Nuts to secure Meter Socket Jaws - (4) 2342702001
Mounting Screws for Meter Socket - (2) 4020508201
Line Side Meter Socket Bus Connectors - 4052722350
Keps Nuts for Line Connectors - (2) 2342702001
Load Side Meter Socket Bus Connectors for LEFT Side Meter Sockets having a wiring gutter located to the right of the tenant circuit breaker
SHORT Bus Connector - 4052720950
LONG Bus Connector - 4052721050
Load Side Meter Socket Bus Connectors for RIGHT Side Meter Sockets having
a wiring gutter located to the left of the tenant circuit breaker
SHORT Bus Connector - 4052721150
LONG Bus Connector - 4052721250
Circuit Breaker Base - 4052720550
Mounting Screws for Circuit Breaker Base - (4 ) 2142717200
Branch Neutral Assembly
Lug Body - 4025110101
Wire Binding Screw - Order Lug No.: 40251-162-51 and use the wire binding screw only from this lug
Mounting Screw for Lug - 2150718200
Bus Connector - 4052717001
Connector Keps Nut - 2342702001

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Individual Meter Socket Trim (Ring Type) - 4052793950
Gasket for Meter Socket Trim - 4052736801
Mounting Screw for Meter Socket Trim - 2142217101
Meter Socket Sealing Ring (standard aluminum snap type) - 2920910001
Circuit Breaker RB Cover (one position) - BCV


CTA-ID : 2047884
Was this helpful?
What can we do to improve the information ?