Technical FAQs

Ask a Question

What is the size and wire range of the lugs in kit number CMELK4?

Issue:
Product Details

Product Line:
Metering Accessory

Cause:
Clarifying wire range

Resolution:
The CMELK4 lug kit includes: (4) ILSCO Lugs, catalog number TA6002N.
Each lug will accommodate (1) #2 AWG - 600 kcmil AL/CU wires and mounts on a lug pad having (2) 1/2" - 13 UNC Studs located on 1.75" centers.
Width of each lug is 1.38" wide.


CTA-ID : 2048038
Was this helpful?
What can we do to improve the information ?