Technical FAQs

Ask a Question

Why does Square D/Schneider Electric not offer a 240V, non-fused Heavy Duty safety switch?

Product features

Product Line:
Heavy Duty Safety Switches

Since the switch would be a Non-Fusible and would NOT provide any overcurrent protection (i.e. NO fuses) there is no reason to have both 240V and 600V. Therefore, Square D/Schneider Electric does not offer a 240V non-fusible version of safety switch because the 600V switch can be used for the 240V application. Fusible safety switches are offered in both 240V and 600V versions due to the differences in the physical size of 240V vs 600V fuses.

CTA-ID : 2047896
Was this helpful?
What can we do to improve the information ?