Technical FAQs

Ask a Question

Can the I-Line TVSS modules be mounted on the right side of the panel?<br />

Advised that it is preferred that the unit be mounted on the left as close to the neutral as possible for best performance however it can be mounted on the right if necessary.

CTA-ID : 2047986
Was this helpful?
What can we do to improve the information ?