Technical FAQs

Ask a Question

Is there a separate incoming main lug for the neutral of a 125amp 3 phase 4 wire NF panel?

Issue:
Is there a separate incoming main lug for the neutral of a 125amp 3 phase 4 wire NF panel?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. On the 125 amp NF panel, the incoming neutral conductor is terminated at the branch neutral bar. The branch neutral bars have termination ports that will accept up to a #2/0 cable.


Revised 4/29/04



CTA-ID : 2048021
Was this helpful?
What can we do to improve the information ?