Technical FAQs

Ask a Question

How long are the leads on the SDSA1175?

The leads are 24 inches. It is recommended to use the shortest lead length possible to offer the maximum surge protection.


CTA-ID : 2047985
Was this helpful?
What can we do to improve the information ?