Technical FAQs

Ask a Question

Is there a dual tandem QO breaker with four 30amp handles on it?

This was an old design and is no longer available. We now offer the QO20303020 which is four handles, two at 20A and two at 30A. For other amperages use two QO1515, two QO2020 or two QO3030 tandem breakers with a handle tie, QOTHT. This uses two pole spaces in the panel. Note these can be used in the old style Non-CTL QO loadcenters only.

CTA-ID : 2047982
Was this helpful?
What can we do to improve the information ?