Technical FAQs

Ask a Question

What amperage of tenant breakers can be used with an EZM125QOA adapter?

The EZM125QOA adaptor will accept only a 2-Pole, QO (40 - 125 ampere), QO-VH (40 - 60 ampere) or QOH (40 - 60 ampere) tenant circuit breaker


CTA-ID : 2047872
Was this helpful?
What can we do to improve the information ?