Technical FAQs

Ask a Question

What is the dimension from the top of the enclosure to the top of the line side lugs on a D326N, Series E03?

There is approximately 14 inches to the line side phase lugs and approximately 25 inches to the line side neutral lug.


CTA-ID : 2047832
Was this helpful?
What can we do to improve the information ?