Technical FAQs

Ask a Question

What is the 480V coil for a CA2DN31T6 IEC Relay?

Issue:
What is the 480V coil for a CA2DN31T6 IEC Relay?

Product Line:
Tesys Relays

Environment:
Obsolete relays

Cause:
Product selection

Resolution:
The LX1D2T6 coil is obsolete. Replace the contactor with the new TeSys product, CAD32T7. Note this is a functional equal only. Accessories for the old product may or may not fit the new design. Confirm dimensions.


CTA-ID : 2048217
Was this helpful?
What can we do to improve the information ?