Technical FAQs

Ask a Question

What are the repair parts for an EZM362R, Series 004, Branch Unit?

ISSUE:
Old design repair parts

PRODUCT LINE:
EZ Meter-Pak Metering Equipment

ENVIRONMENT:
repair parts

CAUSE:
Maintenance

RESOLUTION:
Only the parts listed below are considered field replaceable:

Parts include Meter Socket through Tenant Circuit Breaker Compartment, include quantities for one position only (where a part number only is given the order quantity for that part is one):

5-Jaw Meter Socket - 4052720650 - Obsolete, NLA, With No Replacement
Meter Socket Jaw Assembly - (4) 7329794850
Keps Nuts to secure Meter Socket Jaws - (4) 2342702001
Mounting Screws for Meter Socket - (2) 4020508201
Line Side Meter Socket Bus Connectors - 4052722350 - Obsolete, NLA, With No Replacement
Keps Nuts for Line Connectors - (2) 2342702001
Load Side Meter Socket Bus Connectors for LEFT Side Meter Sockets having a wiring gutter located to the right of the tenant circuit breaker
SHORT Bus Connector - 4052720950
LONG Bus Connector - 4052721050
Load Side Meter Socket Bus Connectors for RIGHT Side Meter Sockets having a wiring gutter located to the left of the tenant circuit breaker
SHORT Bus Connector - 4052721150 - Obsolete, NLA, With No Replacement
LONG Bus Connector - 4052721250 - Obsolete, NLA, With No Replacement
Circuit Breaker Base - 4052720550
Mounting Screws for Circuit Breaker Base - (4 ) 2142717200
Branch Neutral Assembly Lug Body - 4025110101 - Obsolete, NLA, With No Replacement
Wire Binding Screw - Order Lug No.: 4025116251(this is a lug assembly, BUT ONLY the wire binding screw from this lug could be used with the above Obsolete Branch neutral lug. This complete LUG WILL NOT WORK.
Mounting Screw for Lug - 2150718200 - Obsolete, NLA, With No Replacement
Bus Connector - 4052717001 - Obsolete, NLA< With No Replacement
Connector Keps Nut - 2342702001

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Individual Meter Socket Trim (Ring Type) - 4052793950 - Obsolete, NLA, With No Replacement
Gasket for Meter Socket Trim - 4052736801 - Obsolete, NLA, With No Replacement
Mounting Screw for Meter Socket Trim - 2142217101
Meter Socket Sealing Ring (standard aluminum snap type) - 2920910001
Circuit Breaker RB Cover (one position) - BCV - Obsolete, NLA, With No Replacement


CTA-ID : 2047879
Was this helpful?
What can we do to improve the information ?