Technical FAQs

Ask a Question

Is there a series rating available between the NSJ type breakers and the NQ panelboards?

Issue:
Is there a series rating available between the NSJ type breakers and the NQ panelboards?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. The NQ panelboards have no series rating or testing for use with the NSJ Compact type Merlin Gerin breaker.


CTA-ID : 2047928
Was this helpful?
What can we do to improve the information ?