Technical FAQs

Ask a Question

Is the MD50 motor disconnect receptacle compatible with other manufacturers' plugs?

Yes, but they must be an IEC 60309-2 compliant product.


CTA-ID : 2048457
Was this helpful?
What can we do to improve the information ?