Technical FAQs

Ask a Question

If a 30 mm selector switch is installed in the top space of a 9001SKYP Pendant Station, can a gloved hand selector switch knob be used?

A standard 30 mm selector switch will fit in the top space, but with only a standard knob. There is no room or clearance for using the longer gloved hand selector knob.


CTA-ID : 2048398
Was this helpful?
What can we do to improve the information ?