Technical FAQs

Ask a Question

What is the replacement main circuit breaker for a QOBW20M100-5 load center?

Issue:
Repair parts

Product Line:
Obsolete QO LC

Cause:
Maintenance

Resolution:
The QOBW20M100-5 is the box reference number, not the load center catalog number. This box was used with the QO12MW, QO16MW and QO20MW load centers. These load centers used the Q12100TF main circuit breaker, but it is `Obsolete, with no replacement.



CTA-ID : 2048341
Was this helpful?
What can we do to improve the information ?