Technical FAQs

Ask a Question

Are the Powerpact D-frame breakers (DGL DJL and DLL) all the same size?

Yes. They are all 13.38 inches high x 5.51 inches wide x 4.33 inches deep. The different interrupting ratings do not affect the size of the breaker.


CTA-ID : 2047843
Was this helpful?
What can we do to improve the information ?