Technical FAQs

Ask a Question

Is there a motor operator available for the old N frame breakers, such as the NAL, NEL, NXL?<br />

No. The N frame breaker is a 1200 maximum ampere frame device for which there has never been a motor operator available.


CTA-ID : 2048545
Was this helpful?
What can we do to improve the information ?