Technical FAQs

Ask a Question

On Class 9012, what is the definition of maximum allowable pressure?

This is the maximum pressure the switch can handle before rupture of the diaphragm or piston.


CTA-ID : 2048737
Was this helpful?
What can we do to improve the information ?