Technical FAQs

Ask a Question

Are lugs available for the I-Line PL type 1200A breakers that will accommodate 3 - 600 kcmil conductors?

No. The standard I-Line 1200A breaker uses an AL1200P25K lug, which accommodates a maximum of (4) 500 kcmil conductors.

CTA-ID : 2048654
Was this helpful?
What can we do to improve the information ?