Technical FAQs

Ask a Question

What are the lengths of the D11SH10 and D11SH16 shafts for the D10 switch?

D11SH10 - 6-3/8`` including the fitting on the end. For mounting depth of 6 to 10 inches
D11SH16 - 12-1/4`` including the fitting on the end. For mounting depth of 10 to 16 inches.
The customer should refer to the instruction sheet for mounting depth and cutting information.




CTA-ID : 2048400
Was this helpful?
What can we do to improve the information ?