Technical FAQs

Ask a Question

How much current is necessary for the Ammeter trip unit to display current?

Sensor Plug Value (In)
100 to 250 A 30% of Sensor Rating
400 to 1200 A 20% of Sensor Rating
1600 to 6300 A 500 A



CTA-ID : 2048791
Was this helpful?
What can we do to improve the information ?